Increase BLE functionality on the Linux kernel 2.6.31

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Increase BLE functionality on the Linux kernel 2.6.31

1,257 次查看
wangqinghao
Contributor I

Kernel:     linux 2.6.31

Soc:         IMX258

I want to increase the function of BLE,on the IMX 258 platform.How do I increase the Bluez ?Thankyou!

0 项奖励
回复
1 回复

1,160 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

please look at

Bluetoothd (BlueZ 5) won't connect with any devices - www.scriptscoop2.com

heatxsink.com - How to pair a bluetooth device from command line on Linux

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------