Increase BLE functionality on the Linux kernel 2.6.31

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Increase BLE functionality on the Linux kernel 2.6.31

1,250件の閲覧回数
wangqinghao
Contributor I

Kernel:     linux 2.6.31

Soc:         IMX258

I want to increase the function of BLE,on the IMX 258 platform.How do I increase the Bluez ?Thankyou!

0 件の賞賛
返信
1 返信

1,153件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please look at

Bluetoothd (BlueZ 5) won't connect with any devices - www.scriptscoop2.com

heatxsink.com - How to pair a bluetooth device from command line on Linux

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------