Incorrect permissions for Android's root/system after building from sources

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Incorrect permissions for Android's root/system after building from sources

3,717 Views
anon-ac2a625f7b
Contributor I

Hi!

After building Android from sources I get directory structure in out/target/product/...

which contains root/system and other dirs. But when I check permission for dirs/files I see

that all of them are set to local user. As a result (as far as I understand) running it either

using NFS or copying to SD card leads to the situation when Android doesn't boot completely

as well as it doesn't allow to connect to the board via adb. Also it complains about :smileyhappy: permissions.

What I see on the screen attached to the board is A N D R O I D text printed to console by /init (and

no animation etc).

Steps I do for building Android:

0. apply FSL patches

1. source build/envsetup.sh

2. lunch (select platform)

3. make -j8 2>&1 | tee build.log

What am I doing wrong?

Thanks in advance

Andrei.

Labels (2)
0 Kudos
Reply
5 Replies

3,447 Views
anon-ac2a625f7b
Contributor I

So, issue with permissions is solved. Actually, I'm able to boot the board after I extracted ramdisk to sd's root and system.img to /system saving permissions. And what concerns raw directories in "out" directory - as I mentioned before - are still with local user's permissions. So, I assume it's not a bug, it's a feature :smileyhappy:.

0 Kudos
Reply

3,447 Views
saurabh206
Senior Contributor III

Hi

Andrei

Can you try clean build after removing the out directory.

Thanks

Saurabh

0 Kudos
Reply

3,447 Views
anon-ac2a625f7b
Contributor I

Hi, Saurabh

Thanks for answering. Actually I tried a few times. Did the following:

- make installclean

- make clean

and repeated build. But, didn't try to remove out directory completely.

I'll try again and reply here.

addition: "out" removed after doing cleaning steps.

Thanks!

Kind regards,

Andrei.

0 Kudos
Reply

3,447 Views
saurabh206
Senior Contributor III

Hi,

Andrei

Does clean build solved your problem?

0 Kudos
Reply

3,447 Views
anon-ac2a625f7b
Contributor I

Hi, Saurabh!

Merry X-Mas! :smileyhappy:

Nope. Nothing changed.

Here is file/dir list (at pastebin) with user permissions. The same will be for /system directory

http://pastebin.ca/2892285

Regards,

Andrei

0 Kudos
Reply