Inconsistent SPI latencies

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inconsistent SPI latencies

6,797件の閲覧回数
asdaposdi
Contributor I

Hi,

I am running Linux (Yocto) on the Variscite VAR-SOM-MX8M-PLUS (iMX8MP).

I need to stream large amounts of data quickly over SPI, but the time each transfer takes is very inconsistent. In general, I see:

  • a large delay when starting the transfer before the first clock edge (up to hundreds of microseconds),
  • a large delay after the last clock edge before returning from the transfer (up to hundreds of microseconds), and
  • an inconsistent delay between bursts in the same transfer.

In practice, I see that a 2048 byte transfer at 10MHz can take between 2 and 8 ms, where it should take only 8*2048/10MHz = ~1.6ms.

I also occasionally get -ETIMEDOUT, which seems to be the DMA transfer timing out.

I found this thread with similar problems to mine, which provided several solutions that have made some improvements, including isolating a CPU for SPI work.

Am I hitting a hardware limitation? Would moving my SPI interfacing to the Cortex-M core fix this?

Thanks

タグ(3)
0 件の賞賛
返信
4 返答(返信)

5,714件の閲覧回数
mehul_dabhi
Contributor III

Hi @Dhruvit  

I am using the i.MX8MP SoC and have configured the SPI frequency to 25 MHz and 1 am writing 24-bit data. However, I am observing an extended CS (Chip Select) low time of approximately 2.2 µs before the SCLK (Serial Clock) starts, as seen in the captured image.

What steps can I take to reduce the CS low time before the SCLK begins? Any guidance or suggestions

cs_low_time_with_sclk.png

タグ(1)
0 件の賞賛
返信

6,750件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @asdaposdi,

I hope you are doing well.

Could you please share the waveform, and device tree node for further debugging?

Please mention how you are testing it in userspace

The delay between two SPI bursts can be caused by dma limitations.

It seems to be expected behavior.

Yes, Moving SPI interfacing to the Cortex-M core can show improvements.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信

6,723件の閲覧回数
asdaposdi
Contributor I

Hi,

Here's the device tree node:

 

 

#include "imx8mp.dtsi"
&ecspi2 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_ecspi2>;
    status = "okay";
};

 

 

I'm running a kernel module (calling spi_sync_transfer), but I've tested with spidev_test by sending data and measuring on a scope.

Each attachment is a single 2048 byte transfer at 10MHz, including a fast example and a slow example with increasing zoom. I'm just showing the clock so you can see how long the transfer takes.

In fast.png, the clock is continuous with small delays between each byte.

In slow.png, there are large delays every 32 bytes and significant delays between each byte.

Is this the DMA limitation? If so, would the Cortex-M not have the same issue?

Thanks

0 件の賞賛
返信

6,682件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @asdaposdi,

I hope you are doing well.

can you please share the waveform of the CS pin with SCLK.?

Please also mention the kernel version used and chip select information & pinctl.

In DMA mode burst length is limited to word size (32 bits.)

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信