In linux kernel 3.14.28 source we unable to enable following configs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In linux kernel 3.14.28 source we unable to enable following configs.

ソリューションへジャンプ
2,410件の閲覧回数
aravinthkumarja
Senior Contributor II

Following configs can't enable in kernel 3.14.28:-

CONFIG_AC97_BUS

CONFIG_SND_VMASTER

CONFIG_SND_AC97_CODEC

i enabled the "depends on" configs of above mentioned configs, But it's working. Can you please mention the steps to enable the above mentioned configs.

0 件の賞賛
返信
1 解決策
2,297件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi igorpadykov,

Thanks for your response. I can able to configure the above mentioned configuration by enabling CONFIG_SND_SOC_ALL_CODECS

Thanks!

Aravinth

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,298件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi igorpadykov,

Thanks for your response. I can able to configure the above mentioned configuration by enabling CONFIG_SND_SOC_ALL_CODECS

Thanks!

Aravinth

0 件の賞賛
返信
2,295件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi aravinthkumar

SSI driver support AC97 mode, please check ../fsl_ssi.c in

Table 29-1. Stereo Codec SoC Driver Files and sect.29.4.5 Menu

Configuration Options attached Linux Manual.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信