In boota get fastboot lock status error. Set lock status avb_ab_flow.c:30: ERROR: Magic is incorrect.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

In boota get fastboot lock status error. Set lock status avb_ab_flow.c:30: ERROR: Magic is incorrect.

跳至解决方案
3,618 次查看
hongxingyu1982
Contributor III

Hi sir

I used the uuu with the lst script to flash the images, it seems ok, as blew:

flash.png

But it seems can't boot, the error log as blew:

boot.png

Could you give me the solution ?

Thanks

BR

0 项奖励
回复
1 解答
3,393 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Seems like there is a problem with the boot.img, could you please share which Android version you are using?

I assume that you are building your own image, could you please share the procedure you follow to build it?

 

Thank you,

Best regards,

Aldo.

在原帖中查看解决方案

4 回复数
3,394 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Seems like there is a problem with the boot.img, could you please share which Android version you are using?

I assume that you are building your own image, could you please share the procedure you follow to build it?

 

Thank you,

Best regards,

Aldo.

3,392 次查看
hongxingyu1982
Contributor III

Hi AIdo

Thank you very much. Yes,  you are right, it seems the u-boot.img and the boot.img build under the different enviorment, It seems ok when I rebuild all the images under the same enviorment, and download them, it seems ok.

Thanks

BR

0 项奖励
回复
3,392 次查看
hongxingyu1982
Contributor III

Hello everyone

Is there anything update ?

Thanks

BR

0 项奖励
回复
3,392 次查看
hongxingyu1982
Contributor III

Hello

Does everyone meet this issue before ?

BR

0 项奖励
回复