In boota get fastboot lock status error. Set lock status avb_ab_flow.c:30: ERROR: Magic is incorrect.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In boota get fastboot lock status error. Set lock status avb_ab_flow.c:30: ERROR: Magic is incorrect.

Jump to solution
4,465 Views
hongxingyu1982
Contributor III

Hi sir

I used the uuu with the lst script to flash the images, it seems ok, as blew:

flash.png

But it seems can't boot, the error log as blew:

boot.png

Could you give me the solution ?

Thanks

BR

0 Kudos
Reply
1 Solution
4,240 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Seems like there is a problem with the boot.img, could you please share which Android version you are using?

I assume that you are building your own image, could you please share the procedure you follow to build it?

 

Thank you,

Best regards,

Aldo.

View solution in original post

4 Replies
4,241 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Seems like there is a problem with the boot.img, could you please share which Android version you are using?

I assume that you are building your own image, could you please share the procedure you follow to build it?

 

Thank you,

Best regards,

Aldo.

4,239 Views
hongxingyu1982
Contributor III

Hi AIdo

Thank you very much. Yes,  you are right, it seems the u-boot.img and the boot.img build under the different enviorment, It seems ok when I rebuild all the images under the same enviorment, and download them, it seems ok.

Thanks

BR

0 Kudos
Reply
4,239 Views
hongxingyu1982
Contributor III

Hello everyone

Is there anything update ?

Thanks

BR

0 Kudos
Reply
4,239 Views
hongxingyu1982
Contributor III

Hello

Does everyone meet this issue before ?

BR

0 Kudos
Reply