In boota get fastboot lock status error. Set lock status avb_ab_flow.c:30: ERROR: Magic is incorrect.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In boota get fastboot lock status error. Set lock status avb_ab_flow.c:30: ERROR: Magic is incorrect.

ソリューションへジャンプ
3,438件の閲覧回数
hongxingyu1982
Contributor III

Hi sir

I used the uuu with the lst script to flash the images, it seems ok, as blew:

flash.png

But it seems can't boot, the error log as blew:

boot.png

Could you give me the solution ?

Thanks

BR

0 件の賞賛
返信
1 解決策
3,213件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Seems like there is a problem with the boot.img, could you please share which Android version you are using?

I assume that you are building your own image, could you please share the procedure you follow to build it?

 

Thank you,

Best regards,

Aldo.

元の投稿で解決策を見る

4 返答(返信)
3,214件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Seems like there is a problem with the boot.img, could you please share which Android version you are using?

I assume that you are building your own image, could you please share the procedure you follow to build it?

 

Thank you,

Best regards,

Aldo.

3,212件の閲覧回数
hongxingyu1982
Contributor III

Hi AIdo

Thank you very much. Yes,  you are right, it seems the u-boot.img and the boot.img build under the different enviorment, It seems ok when I rebuild all the images under the same enviorment, and download them, it seems ok.

Thanks

BR

0 件の賞賛
返信
3,212件の閲覧回数
hongxingyu1982
Contributor III

Hello everyone

Is there anything update ?

Thanks

BR

0 件の賞賛
返信
3,212件の閲覧回数
hongxingyu1982
Contributor III

Hello

Does everyone meet this issue before ?

BR

0 件の賞賛
返信