In Serial Downloader mode, download using USB, PC does not link to USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In Serial Downloader mode, download using USB, PC does not link to USB

1,337 Views
353533661
Contributor I

In my design, i.mx6ul's UART2_RXD, UART4_RXD, UART5_RXD connected to other MCUs of UART.Internal Boot start-up, i.mx6ul and MCU's UART data communication is no problem.
When in Serial Downloader mode, and this MCU is working, using USB download, the PC does not link to USB.
If the MCU stops working, the PC can link to USB and download it complete.
Is there a BUG in i.mx6ul?

Tags (1)
0 Kudos
Reply
1 Reply

1,287 Views
igorpadykov
NXP Employee
NXP Employee

Hi xiaojun

according to Figure 8-2. Serial Downloader boot flow

i.MX 6UltraLite Applications Processor Reference Manual

both uart and usb are polling by ROM. So uart activity may prevent

PC link to USB.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply