iMX8X mac addresses via uboot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8X mac addresses via uboot?

1,244 Views
mthomas
Contributor I

When I set ethaddr var in uboot I can set an ethernet address for the first Ethernet Port. But how can I set a MAC Address for the second device?

What I have working for the first device is:

...
ethaddr=9C:53:CD:04:A1:12
...

to use ethaddr1 for the second does not work.

0 Kudos
Reply
2 Replies

1,212 Views
mthomas
Contributor I

I found the answer here:
UBootEnvVariables < DULG < DENX 

to set the second device the var is named eth1addr.

0 Kudos
Reply

1,212 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!

0 Kudos
Reply