Imx93 hot-button issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx93 hot-button issue

1,211件の閲覧回数
xiang_1001
Contributor III

The customer wants to transmit hotspots through lte module. After configuring hotspots, use the following command:

iptables -t nat -I POSTROUTING -o ppp0 -j MASQUERADE

 

The mobile phone is connected to the hotspot, indicating that the Internet cannot be accessed.

What else to configure?

0 件の賞賛
返信
2 返答(返信)

1,175件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @xiang_1001 ,

 

By default, i.MX93-EVK supports Murata M.2 WIFI Module based on NXP IW612 chip.

I have 2 question to confirm with you.

(1) WiFi module

Is it NXP IW612 M.2 module?

(2) NAT between WiFi AP and ethernet

You are using iptables to set NAT between WiFi AP and Ethernet? right?

(3) Linux BSP version

If you are using NXP WiFi , please tell me the linux bsp version you are using.

 

Thanks!

Regards,

weidong

 

 

 

0 件の賞賛
返信

1,169件の閲覧回数
xiang_1001
Contributor III

This problem has been solved, thanks.

0 件の賞賛
返信