Imx93 hot-button issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx93 hot-button issue

1,204 Views
xiang_1001
Contributor III

The customer wants to transmit hotspots through lte module. After configuring hotspots, use the following command:

iptables -t nat -I POSTROUTING -o ppp0 -j MASQUERADE

 

The mobile phone is connected to the hotspot, indicating that the Internet cannot be accessed.

What else to configure?

0 Kudos
Reply
2 Replies

1,168 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @xiang_1001 ,

 

By default, i.MX93-EVK supports Murata M.2 WIFI Module based on NXP IW612 chip.

I have 2 question to confirm with you.

(1) WiFi module

Is it NXP IW612 M.2 module?

(2) NAT between WiFi AP and ethernet

You are using iptables to set NAT between WiFi AP and Ethernet? right?

(3) Linux BSP version

If you are using NXP WiFi , please tell me the linux bsp version you are using.

 

Thanks!

Regards,

weidong

 

 

 

0 Kudos
Reply

1,162 Views
xiang_1001
Contributor III

This problem has been solved, thanks.

0 Kudos
Reply