Imx93 hot-button issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx93 hot-button issue

1,212 次查看
xiang_1001
Contributor III

The customer wants to transmit hotspots through lte module. After configuring hotspots, use the following command:

iptables -t nat -I POSTROUTING -o ppp0 -j MASQUERADE

 

The mobile phone is connected to the hotspot, indicating that the Internet cannot be accessed.

What else to configure?

0 项奖励
回复
2 回复数

1,176 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @xiang_1001 ,

 

By default, i.MX93-EVK supports Murata M.2 WIFI Module based on NXP IW612 chip.

I have 2 question to confirm with you.

(1) WiFi module

Is it NXP IW612 M.2 module?

(2) NAT between WiFi AP and ethernet

You are using iptables to set NAT between WiFi AP and Ethernet? right?

(3) Linux BSP version

If you are using NXP WiFi , please tell me the linux bsp version you are using.

 

Thanks!

Regards,

weidong

 

 

 

0 项奖励
回复

1,170 次查看
xiang_1001
Contributor III

This problem has been solved, thanks.

0 项奖励
回复