for hardware side, refer to the material,
−Support up to WXGA@60fps with rich UI & application
−Support up to 1080p@60fps with limited UI update*
−Maximal pixel rate: 150 MP/sec
for the max, you can set 60
for software side, I got document as below:
The LCD driver controller is ili9341, resolution is 320x240, bpp is 16.When SPI bit per word is 32, the performance is 30fps.
so this depends what bpp and what bsp version you use.