Imx6ul use 1280*800 display, how many frames can be displayed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6ul use 1280*800 display, how many frames can be displayed

1,479 次查看
liangmu
Contributor I

Dear ,

I use the imx6ul evk baseline, and the screen resolution is set to 1280*800, and how much is the frame rate set at this time? Will the shadow be displayed?

标签 (1)
0 项奖励
回复
2 回复数

1,321 次查看
joanxie
NXP TechSupport
NXP TechSupport

for hardware side, refer to the material,

  • Display Resolution

Support up to WXGA@60fps with rich UI & application

Support up to 1080p@60fps with limited UI update*

Maximal pixel rate: 150 MP/sec

for the max, you can set 60

for software side, I got document as below:

The LCD driver controller is ili9341, resolution is 320x240, bpp is 16.When SPI bit per word is 32, the performance is 30fps.

so this depends what bpp and what bsp version you use.

0 项奖励
回复

1,321 次查看
liangmu
Contributor I

Thinks for your replay!

In our baseline code,i have find the lcd resolution set to 60fps.

0 项奖励
回复