Imx6 yocto photo display distortion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6 yocto photo display distortion

4,537 Views
chenfeng2016
Contributor I
Hello 
I met a problem on NXP imx6 yocot system, that is the photo display is distorted. The phenomenon is as follows photo files. please helps to analyze what causes it and how to solve it
Version: Linux 4.14.78_.0.0
Thanks.pastedImage_1.png
0 Kudos
Reply
6 Replies

4,357 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

4,357 Views
dioneva_k
Contributor II

What is the value of the vidargs variable in U-Boot?
Use the printenv command to find out
Seems to be low quality video settings

Example of the vidargs variable for iMX6 that I use:
video=mxcfb0:dev=ldb,1280x720M@60,if=RGB888,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=1024M

What is the value of bpp?

Regards,

Dionevã M. Krolow

0 Kudos
Reply

4,357 Views
chenfeng2016
Contributor I

Hello. Dionevã Krolow

   Thanks for your help , according to your vidargs variable, the display work  right.

0 Kudos
Reply

4,357 Views
chenfeng2016
Contributor I

the env parameter  seted as below:

setenv mmcargs 'setenv bootargs ${bootargs} root=/dev/mmcblk3p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'

0 Kudos
Reply

4,357 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which i.MX6 board are you using? Here is your ubuntu system can not work or the system on your i.MX6 board?

0 Kudos
Reply

4,357 Views
chenfeng2016
Contributor I

The board is imx6qp  with the yocto system,

by the way , it has the same phenomenon withe ubuntu system;

0 Kudos
Reply