Imx6 linux + Hypervisor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 linux + Hypervisor

2,683件の閲覧回数
ailtonlopes
Contributor III

Hi, 
I'm working on an trustzone assisted hipervisor (LTZVisor) and i want to run a baremetal OS on the secure World and Linux on the NS Guest.

My question how can i run the linux OS after executing the Startup code and the Hypervisor, now im running the linux using the u-boot as the boot loader and im not sure how to combine both things, the hypervisor and the uboot and linux.

Basically my question is how i can start linux after starting the hypervisor .

Kind regards,

Ailton Lopes

ラベル(2)
0 件の賞賛
返信
1 返信

2,041件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ailton

nxp i.MX6DQ official bsps do not support such use case, one can look on

Boot The i.mx6 dual With Linux+uC/OS-II AMP 

http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf 

https://community.nxp.com/thread/324831#408721 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信