Imx6 Sabre SD - Prebuilt Image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 Sabre SD - Prebuilt Image

3,892件の閲覧回数
prithvi_1506036
Contributor I

Can Someone give the link for Prebuild (*.sdcard.bz) Imx6 Sabre Sd Board's Linux BSP image. I've been searching for the same for more than 2 days. These are the things which I found

1. L4.1.15_1.0.0_MX6QDPSABRESD 

2. Search Results: sabresd 

Images provided in both the Links Doesn't seem to work with my board.. all the custom images which i can build is running properly. I wanted to try booting with the pre buiilt default image for the board and check whether a driver is present or not.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

3,561件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prithvi

right, prebuilt images are specially prepared and built for reference boards

and may not work with custom boards. For custom boards

it is necessary to run ddr test i.MX6/7 DDR Stress Test Tool V3.00 

then rebuild images with new calibration coefficients found from ddr test

(put them in uboot/board/..mx6sabresd/mx6q_4x_mt41j128.cfg).

After loading uboot one can try to use rootfs from prebuilt images.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,561件の閲覧回数
prithvi_1506036
Contributor I

Hi igor,

I'm not using any custom board. I'm using i.MX6QSABRESD https://www.nxp.com/docs/en/user-guide/SABRESDB_IMX6_QSG.pdf

What I'm asking for is that is there any prebuilt images available for the same.. like those which are there for i.MX6QPSABRESD or i.MX6QSOLOX.. etc.

If so, the link for such an image would be appreciated.

Thanks in advance.

0 件の賞賛
返信

3,561件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prithvi

for prebuilt images one can look on

i.MX Software|NXP 

Best regards
igor

0 件の賞賛
返信