Imx6 Quad Part Query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 Quad Part Query

2,321件の閲覧回数
akshatsaraf
Contributor II

Hello,

We are following Sabre for Smart Devices as reference design and making custom board with Imx6 quad processor. In the reference design processor part is PCIMX6Q6AVT10AB, but we want to use the latest part like MCIMX6Q6AVT10AD in our design. I want to know is there any special care we have to taken in the design for the above mentioned part ?

Thanks in Advance.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,109件の閲覧回数
akshatsaraf
Contributor II

Hello,

Can I use MCIMX6Q5EYM10AD part instead of MCIMX6Q6AVT10AD? My design is according to Sabre for Smart Devices board. I have checked both parts are pin compatible, is there any modification in design?

0 件の賞賛
返信

2,109件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Akshat

yes one can use reference design for this part,

PCIMX6Q6AVT10AB is preproduction marking but latest

design i.MX6_SABRE_SDP_DESIGNFILES : Design files, including

hardware schematics is for latest parts (like MCIMX6Q6AVT10AD and others).


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,109件の閲覧回数
akshatsaraf
Contributor II

Thanks igor.

0 件の賞賛
返信