Imx6 Quad Part Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6 Quad Part Query

2,324 Views
akshatsaraf
Contributor II

Hello,

We are following Sabre for Smart Devices as reference design and making custom board with Imx6 quad processor. In the reference design processor part is PCIMX6Q6AVT10AB, but we want to use the latest part like MCIMX6Q6AVT10AD in our design. I want to know is there any special care we have to taken in the design for the above mentioned part ?

Thanks in Advance.

Labels (1)
0 Kudos
Reply
3 Replies

2,112 Views
akshatsaraf
Contributor II

Hello,

Can I use MCIMX6Q5EYM10AD part instead of MCIMX6Q6AVT10AD? My design is according to Sabre for Smart Devices board. I have checked both parts are pin compatible, is there any modification in design?

0 Kudos
Reply

2,112 Views
igorpadykov
NXP Employee
NXP Employee

Hi Akshat

yes one can use reference design for this part,

PCIMX6Q6AVT10AB is preproduction marking but latest

design i.MX6_SABRE_SDP_DESIGNFILES : Design files, including

hardware schematics is for latest parts (like MCIMX6Q6AVT10AD and others).


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,112 Views
akshatsaraf
Contributor II

Thanks igor.

0 Kudos
Reply