Import project(s) from file system MCUXpresso IDE Build Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Import project(s) from file system MCUXpresso IDE Build Error

1,294 Views
bobhi009
Contributor I

Hi,

1. Use "Import SDK example(s)... "Import project 'evkmimxrt1020_lwip_udpecho_freertos' to compile.

2. Delete in Project Explorer (but do not delete the project in the workspace).

3. Use "import project(s) from file system" to import the project from the workspace again.

4. The compilation fails

bobhi009_0-1680839283625.png

 

0 Kudos
Reply
3 Replies

1,252 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

I made a same test but didn't see the problem. What's the version of MCUXpresso and SDK?

 

Regards,

Jing

0 Kudos
Reply

1,242 Views
bobhi009
Contributor I

MCUXpresso IDE v11.5.1 and SDK_2_11_0_EVK-MIMXRT1020

It seems that only projects that include lwip have this problem.

0 Kudos
Reply

1,239 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

You can try to update IDE to 11.7.

 

Regards,

Jing

0 Kudos
Reply