Import project(s) from file system MCUXpresso IDE Build Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import project(s) from file system MCUXpresso IDE Build Error

1,939件の閲覧回数
bobhi009
Contributor I

Hi,

1. Use "Import SDK example(s)... "Import project 'evkmimxrt1020_lwip_udpecho_freertos' to compile.

2. Delete in Project Explorer (but do not delete the project in the workspace).

3. Use "import project(s) from file system" to import the project from the workspace again.

4. The compilation fails

bobhi009_0-1680839283625.pngbobhi009_0-1680839283625.png

 

0 件の賞賛
返信
3 返答(返信)

1,897件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

I made a same test but didn't see the problem. What's the version of MCUXpresso and SDK?

 

Regards,

Jing

0 件の賞賛
返信

1,887件の閲覧回数
bobhi009
Contributor I

MCUXpresso IDE v11.5.1 and SDK_2_11_0_EVK-MIMXRT1020

It seems that only projects that include lwip have this problem.

0 件の賞賛
返信

1,884件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

You can try to update IDE to 11.7.

 

Regards,

Jing

0 件の賞賛
返信