Implementing the avb stack on imx6 sabre auto with full ubuntu rootfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Implementing the avb stack on imx6 sabre auto with full ubuntu rootfs

1,119 次查看
ajayvenkatakris
Contributor II

Hi, 

      Is it possible to implement the open source AVB stack available on github in the IMX6DL Sabre auto board which runs the full Ubuntu Rootfs?

标签 (6)
0 项奖励
回复
1 回复

867 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ajay

may be useful to look at presentation on

https://community.nxp.com/docs/DOC-333044

also one can post on meta-fsl-arm mailing list, so that someone familiar with

open source AVB implementations could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复