Image shift right for LVDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Image shift right for LVDS

1,385件の閲覧回数
hankwang
Contributor V

Hi, I have a problem.  I use the sn65dsi8x dirver to enable LVDS signal. I can see the image, but image shift right.

I can modify which parameter to fix this problem ? I have tried the hfront_porch , hback_porch, but the problem is not fix.

S__24444930.jpg

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

976件の閲覧回数
sabidi
Contributor I

Hi,

I'am working with imx8mm using sn65dsi83 and ihave the same issue, can you please share the solution?

0 件の賞賛
返信

1,317件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hank

one can look at below variscite guidelines for adding custom panel. also

pay attention to proper panel initialization, function rad_panel_push_cmd_list() in

panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

DART-MX8M Display - Variscite Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信