ITU-R BT.656 Digital Video Interface connection with i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ITU-R BT.656 Digital Video Interface connection with i.MX6SL

Jump to solution
3,620 Views
ko-hey
Senior Contributor II

Hi all

I want to confirm a connection of i.MX6SL with LCD.

My customer want to use eLCDIF in ITU-R BT.656 Digital Video Interface.

So we read section 21.4.11 and 21.4.12 in reference manual but can not understand it.

We understand that they need to connect only data and clock.

However, we can't figure out that which pin can we use as a clock signal.

Which pin can we use ?

i.MX 6SoloLite Applications Processor Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf

Ko-hey

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
3,255 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.

Pin use in DOTCLK Mode and DVI Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,256 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.

Pin use in DOTCLK Mode and DVI Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,255 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for reply.

In other words, we should use LCD_DOTCLK pin to provide a clock.

Is it correct ?

Ko-hey

0 Kudos
Reply
3,255 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

one needs to use signal LCD_RS, pad LCD_VSYNC(ALT2)

check Table 4-1. Pin Assignments i.MX6SL RM

Best regards

igor

3,255 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your support.

Ko-hey

0 Kudos
Reply