ITU-R BT.656 Digital Video Interface connection with i.MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ITU-R BT.656 Digital Video Interface connection with i.MX6SL

跳至解决方案
3,623 次查看
ko-hey
Senior Contributor II

Hi all

I want to confirm a connection of i.MX6SL with LCD.

My customer want to use eLCDIF in ITU-R BT.656 Digital Video Interface.

So we read section 21.4.11 and 21.4.12 in reference manual but can not understand it.

We understand that they need to connect only data and clock.

However, we can't figure out that which pin can we use as a clock signal.

Which pin can we use ?

i.MX 6SoloLite Applications Processor Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf

Ko-hey

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,258 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.

Pin use in DOTCLK Mode and DVI Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,259 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

it is LSD_RS (CCIR_CLK) as depicted in Table 21-4.

Pin use in DOTCLK Mode and DVI Mode

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,258 次查看
ko-hey
Senior Contributor II

Hi Igor

Thank you for reply.

In other words, we should use LCD_DOTCLK pin to provide a clock.

Is it correct ?

Ko-hey

0 项奖励
回复
3,258 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

one needs to use signal LCD_RS, pad LCD_VSYNC(ALT2)

check Table 4-1. Pin Assignments i.MX6SL RM

Best regards

igor

3,258 次查看
ko-hey
Senior Contributor II

Hi Igor

Thank you for your support.

Ko-hey

0 项奖励
回复