ISO/IEC 5230:2020 certification confirmation for i.MX software.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISO/IEC 5230:2020 certification confirmation for i.MX software.

Jump to solution
2,697 Views
Yoshidaj
Contributor I

Customer request NXP to confirm for the certification ISO/IEC 5230:2020 ( OSS Compliance ).

We cannot confirm that the NXP i.MX Linux/ Android BSP was certified for OSS compliance, would you kindly let us know the NXP software certification status for OSS ?

*The attached file is OSS leaflet.

If NXP doesn't have its certification, also let us know the plan to acquire its certification.

Labels (1)
0 Kudos
Reply
1 Solution
2,661 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi @Yoshidaj,

 

Please open a case as the info can't be shared on the community, mention this community thread and I will answer there.

 

Regards,

Israel.

View solution in original post

2 Replies
2,662 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi @Yoshidaj,

 

Please open a case as the info can't be shared on the community, mention this community thread and I will answer there.

 

Regards,

Israel.

2,648 Views
Yoshidaj
Contributor I

Dear Israel.

Thanks for your reply. We also put question on TIC and check it.

Yoshida

0 Kudos
Reply