ISO/IEC 5230:2020 certification confirmation for i.MX software.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ISO/IEC 5230:2020 certification confirmation for i.MX software.

跳至解决方案
2,699 次查看
Yoshidaj
Contributor I

Customer request NXP to confirm for the certification ISO/IEC 5230:2020 ( OSS Compliance ).

We cannot confirm that the NXP i.MX Linux/ Android BSP was certified for OSS compliance, would you kindly let us know the NXP software certification status for OSS ?

*The attached file is OSS leaflet.

If NXP doesn't have its certification, also let us know the plan to acquire its certification.

标签 (1)
0 项奖励
回复
1 解答
2,663 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi @Yoshidaj,

 

Please open a case as the info can't be shared on the community, mention this community thread and I will answer there.

 

Regards,

Israel.

在原帖中查看解决方案

2 回复数
2,664 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi @Yoshidaj,

 

Please open a case as the info can't be shared on the community, mention this community thread and I will answer there.

 

Regards,

Israel.

2,650 次查看
Yoshidaj
Contributor I

Dear Israel.

Thanks for your reply. We also put question on TIC and check it.

Yoshida

0 项奖励
回复