IPU csi0 test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPU csi0 test

2,059件の閲覧回数
zhiyuan_song
Contributor II

hi,I have a problem. I use the ipucsi test pattern,set csi0 test control register

csi->smfc->idmac

first: idmac configuration

void ipu_general_idmac_config()
{
 uint32_t channel = 0;
 /* enable channel 0 */
 ipu_idmac_channel_enable(channel, 0);
 memset((void *)ipu_cpmem_addr(channel), 0, sizeof(ipu_cpmem_t));
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 0, 29, 0x07000000);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 29, 29, 0);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 125, 13, 0x0000027f);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 138, 12, 0x000001df);
    /*setup default pixel format */
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 85, 4, INTERLEAVED_RGB565);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 107, 3, 3);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 116, 3, 5 - 1);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 119, 3, 6 - 1);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 122, 3, 5 - 1);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 125, 3, 0 - 1);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 128, 5, 0);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 133, 5, 5);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 138, 5, 11);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 143, 5, 16);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 102, 14, 640 - 1);

    /*setup pixel per burst */
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 78, 7, 15);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 113, 1, 0);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 1, 58, 20, 0);
    //setup rotate/vf/hf and block mode
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 119, 1, 0);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 121, 1, 0);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 120, 1, 0);
    ipu_cpmem_set_field(ipu_cpmem_addr(channel), 0, 117, 2, 0);
    ipu_idmac_channel_mode_sel(channel, 0);
    ipu_idmac_channel_enable1(channel, 1);
}

 Then, SMFC configuration:

uint32_t ipu_smfc_fifo_allocate(uint32_t channel, uint32_t map,
                                uint32_t burst_size)
{
    switch (channel) {
    case 0:
        writel(map, 0x2650000);//smfc map
        writel(burst_size, 0x2650008);//smfc bs
        break;
    case 1:
        writel(map, 0x2650000);
        writel(burst_size, 0x2650008);
        break;
    case 2:
        writel(map, 0x2650000);
        writel(burst_size, 0x2650008);
        break;
    case 3:
        writel(map, 0x2650000);
        writel(burst_size, 0x2650008);
        break;
    default:
        printf("Wrong channel selected!!\n");
        return -1;
    }
    writel(1 << 8, 0x2600000);//enable smfc
    return 0;
}
and the csi configuration :
void ipu_csi_config()
{
 //test
 writel(1 << 24, 0x2630010);//enable test
 //writel((readl(0x2600000) | 1 << 28), 0x2600000);//mipi
 //writel(0x1e, 0x2638020);//di
 writel(((0 << 31) | (1 << 15) | (0 << 3) | (0 << 2) | (0x4 << 24) | (1 << 4) | (0x9f << 16)), 0x2630000);
 //writel(((0x04 << 24) | (0x00 << 4) | (0x0 << 16) | (0x1 << 11) | (0x0 << 7) | (0x02 << 8)), 0x2630000);
 writel(((0x01df << 16) | (0x027f << 0)), 0x2630004);
 writel((readl(0x2600000) | (1 << 0)), 0x2600000);//enable csi0
} 
void ipu_buffer()
{
 writel(readl(0x26000e4) | (0 << 28), 0x26000e4);
 writel(readl(0x2600268) | 1, 0x2600268);
 writel(readl(0x26000e4) | (0 << 30), 0x26000e4);
 writel(readl(0x2600270) | 1, 0x2600270);
}
void ipu_capture_setup(uint32_t ipu_index, uint32_t csi_interface, uint32_t raw_width,
                       uint32_t raw_height, uint32_t act_width, uint32_t act_height)
{
 uint32_t csi_mem0 = 0x40000000, csi_mem1 = 0;
 int32_t csi_pixel_format = NON_INTERLEAVED_YUV420;
    if (csi_interface == CSI_TEST_MODE)
        csi_pixel_format = INTERLEAVED_RGB565;
    // put csi captured image into memory first
    ipu_general_idmac_config();
    /*step2: allocate smfc fifo for CSI input channel */
    ipu_smfc_fifo_allocate(0, 0, 3);
    /*step3: config csi for IPU */
    ipu_csi_config();
    memset((void *)csi_mem0, 0xFF, 640 * 480 * 2);
    ipu_buffer();
}
My test function is as follows:
int32_t csi_test_mode()
{
 int32_t ipu_index = 1, count = 0;
 int32_t width = 640, height = 480;
 /*step 2: setup IPU: from csi to display */
 ipu1_iomux_config();
 ipu_sw_reset(ipu_index, 1000);
 ipu_capture_setup(ipu_index, CSI_TEST_MODE, width, height, width, height);
 while(1){
  ipu_csi_test_mode_color(ipu_index, (count++) % 8);
 }
}
Why can't I get the generated checkerboard image?
I looked at the memory at 0x08000000 and 0x40000000,I find that the data is constant.0x40000000 looks random
0x08000000 looks regular.data:0x38613860 0x38653864 0x38693868 0x386d386c...
Can you help me?
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,977件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi song

for ipu csi test pattern example one can check function ipu_csi_test_mode() in

rt-thread/ipu_csi.c at master · RT-Thread/rt-thread · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,977件の閲覧回数
zhiyuan_song
Contributor II

hi,igorpadykov,IPU channel 0 interrupt flag bit has become one, how to reset it?

0 件の賞賛
返信