IPG/PER clocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,347件の閲覧回数
vsiles
Senior Contributor I

Hi !

I've tried to search for the meaning of the 'IPG' acronym that one can find in several reference manual or in Linux source code, but I can't find a source. What does 'IPG' stands for ?

Also, I'm trying to fully understand the differences between the 'ipg' and 'per' clocks that most device have (for in Linux dtb). My understanding is that the 'ipg' clock drives the access to the device iomapped registers, and the 'per' clocks drives the device itself.

Am I right ?

Thank your for your explanation,

V.

ラベル(3)
1 解決策
5,285件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

yes this is right. Seems 'IPG' relates to IPbus global clock (IP Bus Interface (AIPI)).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
5,286件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

yes this is right. Seems 'IPG' relates to IPbus global clock (IP Bus Interface (AIPI)).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,285件の閲覧回数
vsiles
Senior Contributor I

Thank you !

0 件の賞賛
返信