IMx 6 usb debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMx 6 usb debugger

1,881件の閲覧回数
kalai
Contributor I

hi,

 

  i am using imx6sx sabrese sd board. i need to know about debug using usb without any debugger module.

if any IDE available for debug without debugger

how to run the board without memory card?

 

thanks

kalai

0 件の賞賛
返信
3 返答(返信)

1,863件の閲覧回数
kalai
Contributor I

Hi

Will MCUXpresso IDE supports for I.MX 6 series?

 

Regards,

Kalai

0 件の賞賛
返信

1,854件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kalai 
Hello,

  MCUXpresso IDE does not support i.MX6.

Regards,
Yuri,

0 件の賞賛
返信

1,875件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kalai 
Hello,

We do not have recommendations regarding debug IDE over USB.
Usually JTAG (Lauterbach, ARM DS-5 DSTREAM) is applied.
Customer can try using relatively simple command line application,
such as sdphost. The sdphost tool provides a command line interface
for sending Serial Download Protocol (SDP) commands from the PC host
to NXP i.MX devicesin the serial download mode.

You may look at section 4.2.1 (SDPHost downloads Flashloader image)
of the following app note reagrding example how to use it.

 https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf

 

Regards,
Yuri.

0 件の賞賛
返信