IMx 6 usb debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMx 6 usb debugger

1,871 Views
kalai
Contributor I

hi,

 

  i am using imx6sx sabrese sd board. i need to know about debug using usb without any debugger module.

if any IDE available for debug without debugger

how to run the board without memory card?

 

thanks

kalai

0 Kudos
Reply
3 Replies

1,853 Views
kalai
Contributor I

Hi

Will MCUXpresso IDE supports for I.MX 6 series?

 

Regards,

Kalai

0 Kudos
Reply

1,844 Views
Yuri
NXP Employee
NXP Employee

@kalai 
Hello,

  MCUXpresso IDE does not support i.MX6.

Regards,
Yuri,

0 Kudos
Reply

1,865 Views
Yuri
NXP Employee
NXP Employee

@kalai 
Hello,

We do not have recommendations regarding debug IDE over USB.
Usually JTAG (Lauterbach, ARM DS-5 DSTREAM) is applied.
Customer can try using relatively simple command line application,
such as sdphost. The sdphost tool provides a command line interface
for sending Serial Download Protocol (SDP) commands from the PC host
to NXP i.MX devicesin the serial download mode.

You may look at section 4.2.1 (SDPHost downloads Flashloader image)
of the following app note reagrding example how to use it.

 https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf

 

Regards,
Yuri.

0 Kudos
Reply