IMXRT1176 evk running from SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1176 evk running from SDRAM

Jump to solution
1,378 Views
ahmedhrabi
Contributor IV

Hi all, 

I'am trying to run an SDK example (evkmimxrt1170_lvgl_demo_widgets_cm7) on imxrt1176 evk board, from the external ram SDRAM.

here's my config : 

SDRAM conf.png

The example crash with this conf, did someone have an idea about that ? 

Another question, when running the app from SDRAM can i debug through CMSIS-DAP linkserver or with PE Multilink ? 

Regards. 

Tags (2)
0 Kudos
Reply
1 Solution
1,364 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @ahmedhrabi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, regarding the MCU settings, just clicking the Link application to RAM is enough, further, follow the post to set up the script to enable the debug in the SDRAM.

jeremyzhou_0-1658891006158.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

2 Replies
1,361 Views
ahmedhrabi
Contributor IV

Hi @jeremyzhou

It works. Thank you for your support.

Regards.

0 Kudos
Reply
1,365 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @ahmedhrabi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, regarding the MCU settings, just clicking the Link application to RAM is enough, further, follow the post to set up the script to enable the debug in the SDRAM.

jeremyzhou_0-1658891006158.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------