IMXRT1176 evk running from SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1176 evk running from SDRAM

ソリューションへジャンプ
1,355件の閲覧回数
ahmedhrabi
Contributor IV

Hi all, 

I'am trying to run an SDK example (evkmimxrt1170_lvgl_demo_widgets_cm7) on imxrt1176 evk board, from the external ram SDRAM.

here's my config : 

SDRAM conf.png

The example crash with this conf, did someone have an idea about that ? 

Another question, when running the app from SDRAM can i debug through CMSIS-DAP linkserver or with PE Multilink ? 

Regards. 

タグ(2)
0 件の賞賛
返信
1 解決策
1,341件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @ahmedhrabi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, regarding the MCU settings, just clicking the Link application to RAM is enough, further, follow the post to set up the script to enable the debug in the SDRAM.

jeremyzhou_0-1658891006158.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

元の投稿で解決策を見る

2 返答(返信)
1,338件の閲覧回数
ahmedhrabi
Contributor IV

Hi @jeremyzhou

It works. Thank you for your support.

Regards.

0 件の賞賛
返信
1,342件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @ahmedhrabi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, regarding the MCU settings, just clicking the Link application to RAM is enough, further, follow the post to set up the script to enable the debug in the SDRAM.

jeremyzhou_0-1658891006158.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------