IMXRT1150 EVK(Rev C3)-QSPI Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1150 EVK(Rev C3)-QSPI Bootloader

2,486 Views
Arivuvp
Contributor I

As of now , i have one sample bin file,How can i write with in QSPI bootloder ,and its When ever Started code boot from Qspi ..

0 Kudos
Reply
4 Replies

2,480 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Arivuvp ,

  I think you mention MIMXRT1050-EVKB board, please help to check the board at first.

Or you can give me your board photo, then I can help you to check the details.

  At first, you need to make sure your board hardware is using the QSPI, then you can do the QSPI flash boot, RT1050-EVKB is using the hyperflash in default, so, if you want to use the QSPI, you need to modify the hardware resistor to select the QSPI flash.

 About the detail QSPI flash usage, please refer to this application note:

https://www.nxp.com/docs/en/application-note/AN12108.pdf

 

Wish it helps you!
Best Regards,

Kerry

0 Kudos
Reply

2,476 Views
Arivuvp
Contributor I

sorry..I am using  IMXRT1170 EVK board  not 1050 ..

0 Kudos
Reply

2,472 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Arivuvp ,

  If you are using the MIMXRT1170-EVK board, it's more easy, as it is just the QSPI flash boot directly.

  About the code, please refer to the SDK code, all the SDK demo are booting from the QSPI flash.

  You can download the SDK code from this link:

https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1170-EVK

  You can run this simple demo directly:

SDK_2_12_0_MIMXRT1170-EVK\boards\evkmimxrt1170\demo_apps\led_blinky\cm7

 

If you meet any issues, you can refer to the doc in the SDK:

\SDK_2_12_0_MIMXRT1170-EVK\docs\Getting Started with MCUXpresso SDK for MIMXRT1170-EVK.pdf

 

Wish it helps you!
Best Regards,

kerry

0 Kudos
Reply

2,477 Views
Arivuvp
Contributor I

Please find attached board photo..And i have followed (https://community.nxp.com/t5/i-MX-RT/i-MX-RT1170-with-MCU-Boot-Utility/td-p/1303418) this procedure.IMXRT1170_EVK.jpg

0 Kudos
Reply