IMXRT1150 EVK(Rev C3)-QSPI Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1150 EVK(Rev C3)-QSPI Bootloader

2,424件の閲覧回数
Arivuvp
Contributor I

As of now , i have one sample bin file,How can i write with in QSPI bootloder ,and its When ever Started code boot from Qspi ..

0 件の賞賛
返信
4 返答(返信)

2,418件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Arivuvp ,

  I think you mention MIMXRT1050-EVKB board, please help to check the board at first.

Or you can give me your board photo, then I can help you to check the details.

  At first, you need to make sure your board hardware is using the QSPI, then you can do the QSPI flash boot, RT1050-EVKB is using the hyperflash in default, so, if you want to use the QSPI, you need to modify the hardware resistor to select the QSPI flash.

 About the detail QSPI flash usage, please refer to this application note:

https://www.nxp.com/docs/en/application-note/AN12108.pdf

 

Wish it helps you!
Best Regards,

Kerry

0 件の賞賛
返信

2,414件の閲覧回数
Arivuvp
Contributor I

sorry..I am using  IMXRT1170 EVK board  not 1050 ..

0 件の賞賛
返信

2,410件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Arivuvp ,

  If you are using the MIMXRT1170-EVK board, it's more easy, as it is just the QSPI flash boot directly.

  About the code, please refer to the SDK code, all the SDK demo are booting from the QSPI flash.

  You can download the SDK code from this link:

https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1170-EVK

  You can run this simple demo directly:

SDK_2_12_0_MIMXRT1170-EVK\boards\evkmimxrt1170\demo_apps\led_blinky\cm7

 

If you meet any issues, you can refer to the doc in the SDK:

\SDK_2_12_0_MIMXRT1170-EVK\docs\Getting Started with MCUXpresso SDK for MIMXRT1170-EVK.pdf

 

Wish it helps you!
Best Regards,

kerry

0 件の賞賛
返信

2,415件の閲覧回数
Arivuvp
Contributor I

Please find attached board photo..And i have followed (https://community.nxp.com/t5/i-MX-RT/i-MX-RT1170-with-MCU-Boot-Utility/td-p/1303418) this procedure.IMXRT1170_EVK.jpg

0 件の賞賛
返信