IMXRT1024-EVK Ethernet CRS Routing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1024-EVK Ethernet CRS Routing

1,303件の閲覧回数
GUnderdown
Contributor IV

On the EVK for the xx1024, the schematic shows the ENET_CRS_DV pin being routed from the PHY (U11) to the CPU on pin 97 (GPIO_AD_B0_11). The reference manual (p261) says that the ENET_CRS signal must be routed to GPIO_EMC_34.

 

Is this an error in the eval board? Which pin should this signal be routed to?

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,254件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

From RT1024 reference manual page1734 Table 37-44 ENET External Signals description:

ENET_CRS (GPIO_EMS_34 pad) signal only works for MII mode:

Hui_Ma_0-1686553108337.png

RT1024 EVK board ENET works at RMII mode, which using RX_EN (GPIO_AD_B0_11 pad) signal as CRS_DV input signal.

Hui_Ma_1-1686553272229.png

So, the RT1024 EVK board ENET_CRS_DV connection is correct.

best regards,

Mike

  

0 件の賞賛
返信