IMXRT1024-EVK Ethernet CRS Routing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1024-EVK Ethernet CRS Routing

1,288 Views
GUnderdown
Contributor IV

On the EVK for the xx1024, the schematic shows the ENET_CRS_DV pin being routed from the PHY (U11) to the CPU on pin 97 (GPIO_AD_B0_11). The reference manual (p261) says that the ENET_CRS signal must be routed to GPIO_EMC_34.

 

Is this an error in the eval board? Which pin should this signal be routed to?

 

Labels (1)
0 Kudos
Reply
1 Reply

1,239 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

From RT1024 reference manual page1734 Table 37-44 ENET External Signals description:

ENET_CRS (GPIO_EMS_34 pad) signal only works for MII mode:

Hui_Ma_0-1686553108337.png

RT1024 EVK board ENET works at RMII mode, which using RX_EN (GPIO_AD_B0_11 pad) signal as CRS_DV input signal.

Hui_Ma_1-1686553272229.png

So, the RT1024 EVK board ENET_CRS_DV connection is correct.

best regards,

Mike

  

0 Kudos
Reply