IMX93 Enabling USART flow control (DCD, DSR, DTR, RTS, CTS)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93 Enabling USART flow control (DCD, DSR, DTR, RTS, CTS)

4,695件の閲覧回数
wcastidex
Contributor I

Hello, 

 

Currently trying to enable full hardware flow control on LPUART4 on a iMX93, I've had success enabling RTS and CTS but haven't been able to get DSR,  DCD, and DTR enabled.  

My DT pins are defined as follows:

 

pinctrl_uart4: uart4grp {
fsl,pins = <
MX93_PAD_ENET2_RD0__LPUART4_RX 0x31e
MX93_PAD_ENET2_TD0__LPUART4_TX 0x31e
MX93_PAD_ENET2_TD1__LPUART4_RTS_B 0x31e
MX93_PAD_ENET2_RD2__LPUART4_CTS_B 0x31e
MX93_PAD_ENET2_RX_CTL__LPUART4_DSR_B 0x31e
MX93_PAD_ENET2_TX_CTL__LPUART4_DTR_B 0x31e
>;
};

 

 
 
and 
 

 

lpuart4: serial@42580000 {
compatible = "fsl,imx93-lpuart", "fsl,imx8ulp-lpuart", "fsl,imx7ulp-lpuart";
reg = <0x42580000 0x1000>;
interrupts = <GIC_SPI 69 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX93_CLK_LPUART4_GATE>;
clock-names = "ipg";
dmas = <&edma2 19 0 0>, <&edma2 20 0 1>;
dma-names = "tx","rx";
uart-has-rtscts;
status = "ok";
};

 

but when looking at the driver it doesnt seem to recognize RTS or DTR and I don't have a pin available for DCD. 
 

 

]# cat /proc/tty/driver/fsl-lpuart
serinfo:1.0 driver revision:
0: uart:FSL_LPUART mmio:0x44380010 irq:18 tx:12447 rx:43 RTS|CTS|DTR|DSR|CD
1: uart:FSL_LPUART mmio:0x42690010 irq:24 tx:0 rx:0 CTS|DSR|CD
2: uart:FSL_LPUART mmio:0x42570010 irq:20 tx:0 rx:0 CTS|DSR|CD
3: uart:FSL_LPUART mmio:0x42580010 irq:21 tx:0 rx:0 CTS|DSR|CD
4: uart:FSL_LPUART mmio:0x42590010 irq:22 tx:0 rx:0 CTS|DSR|CD
5: uart:FSL_LPUART mmio:0x425A0010 irq:23 tx:0 rx:0 CTS|DSR|CD
6: uart:FSL_LPUART mmio:0x44390010 irq:19 tx:0 rx:0 CTS|DSR|CD

 

 

I've looked through imx93-pinfunc.h for DCD but dont see an assignment, which is okay we can do it with a GPIO if needed but looking at page 4978 of IMX93RM it appears that the MODEM control register supports a DCD pin mapping.  
 
Looking through some of the other nxp devtree files I have seen a reference to a device tree option such as rts-gpios, cts-gpios, dtr-gpios, dsr-gpios, and dcd-gpios but it appears this is assigning those pins as a gpio to be handled in software and not to the peripheral device?  
 
Confusingly uart0 is my debug port and it has all pins activated yet those pins aren't defined in my device tree and are not wired up on my hardware.  
 
I've searched through kernel message log to make sure there were no pin assignment conflicts as well.
 
Any help is appreciated,
 
Thank you,
Walter
 
ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

4,651件の閲覧回数
matato
Contributor I

 

The serial port program is a standard program. Have you configured the serial port properties according to the ioctl provided by the Linux standard program?

Or use stty to set it?

#include <stdio.h>
#include <fcntl.h>
#include <unistd.h>
#include <sys/ioctl.h>
#include <termios.h>

int main() {
    int fd = open("/dev/ttyS0", O_RDWR); // Change to the correct serial port
    if (fd == -1) {
        perror("open");
        return 1;
    }

    int status;
    
    // Get current modem control lines
    ioctl(fd, TIOCMGET, &status);
    
    // Enable DTR (Data Terminal Ready)
    status |= TIOCM_DTR;
    
    // Apply new settings
    ioctl(fd, TIOCMSET, &status);

    printf("DTR enabled.\n");

    close(fd);
    return 0;
}

 

 

0 件の賞賛
返信

4,672件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @wcastidex!

Thank you for contacting NXP Support!

 

Unfortunately those functions are not implemented in the driver but the kernel can manage those functions using gpios instead.

 

You can add the next lines to your device tree:

	dtr-gpios = <&gpio4 3 GPIO_ACTIVE_LOW>;
	dsr-gpios = <&gpio4 4 GPIO_ACTIVE_LOW>;
	dcd-gpios = <&gpio4 6 GPIO_ACTIVE_LOW>;

#Example

 

 

Best Regards!

Chavira

0 件の賞賛
返信

4,656件の閲覧回数
lapohab
Contributor III

 

gpio cts and rts can be used because the driver implements this function and calls the API provided by serial_mctrl_gpio.c, such as imx.c, another driver of imx.

However, fsl_lpuart.c does not see the API provided by serial_mctrl_gpio.c being called.

In addition, if uart-has-rtscts is not removed, even if the gpio control you mentioned is added, it will not work. Because the serial bindings have uart-has-rtscts; it means that the rts cts of the serial controller is used.

 

serial.yaml

uart-has-rtscts:
$ref: /schemas/types.yaml#/definitions/flag
description:
The presence of this property indicates that the UART has dedicated lines
for RTS/CTS hardware flow control, and that they are available for use
(wired and enabled by pinmux configuration). This depends on both the
UART hardware and the board wiring.


https://github.com/nxp-imx/linux-imx/blob/lf-6.6.52-2.2.0/drivers/tty/serial/serial_mctrl_gpio.c


https://github.com/nxp-imx/linux-imx/tree/lf-6.6.52-2.2.0/drivers/tty/serial/fsl_lpuart.c

https://github.com/nxp-imx/linux-imx/tree/lf-6.6.52-2.2.0/drivers/tty/serial/imx.c

/* called with port.lock taken and irqs caller dependent */
static void imx_uart_rts_active(struct imx_port *sport, u32 *ucr2)
{
	*ucr2 &= ~(UCR2_CTSC | UCR2_CTS);

	mctrl_gpio_set(sport->gpios, sport->port.mctrl | TIOCM_RTS);
}

/* called with port.lock taken and irqs caller dependent */
static void imx_uart_rts_inactive(struct imx_port *sport, u32 *ucr2)
{
	*ucr2 &= ~UCR2_CTSC;
	*ucr2 |= UCR2_CTS;

	mctrl_gpio_set(sport->gpios, sport->port.mctrl & ~TIOCM_RTS);
}
0 件の賞賛
返信

4,553件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi all!

 

The fsl-lpuart driver only can manage the cts and rts pins from hardware.

since the other signals are not commonly used are not implemented in our driver but our hardware is capable to manage those signals.

 

As you mention, declaring the pins on device tree the Kernel is not solving the signals and for that case we have to do it manually in a c or python program.

 

Best Regards!

Chavira

0 件の賞賛
返信