Create frame buffer without hdmi device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create frame buffer without hdmi device

Jump to solution
1,576 Views
kluszon
Contributor III
  • Processor: iMX8M
  • System: Yocto with Wayland 

I would like to play video immediately after the system starts. However, I encounter a problem when the HDMI cable isn't connected during system startup. In this situation, a frame buffer isn't created, which is correct in the normal situation. I can't start playing such situation.  Is there any way to create a frame buffer with specified resolution without detecting the HDMI device? The approach should continue to play the video after connecting the cable on a compatible screen.

Tags (3)
0 Kudos
Reply
1 Solution
1,533 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately no, for video to continue to be played needs a sink (display).

Best regards/Saludos,
Aldo.

View solution in original post

1 Reply
1,534 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately no, for video to continue to be played needs a sink (display).

Best regards/Saludos,
Aldo.