IMX93 Boot Status Not updating based on watchdog reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX93 Boot Status Not updating based on watchdog reset

1,618件の閲覧回数
vinisha
Contributor I

Hello NXP Engineers,

Board under use: NXP provided IMX93EVK board.

We are running a Watchdog_demo code using which we are able to triggre the watchdog and watchdog reset works with in the expected timeout period. But In the next boot when we check the BOOT STATUS It always provides POR(Power On Reset).

I would Like to know why the Boot status is not getting updated when the board is booted based on watchdog.

Best regards,

Vinisha

0 件の賞賛
返信
6 返答(返信)

1,594件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

 

The WDG signal on EVK board will trigger cold reset.

Zhiming_Liu_0-1731463714925.png



Best Regards,
Zhiming

0 件の賞賛
返信

1,578件の閲覧回数
vinisha
Contributor I

Hello Zhiming,

I appreciate your prompt reply. According to your response, the reset that was seen was a cold reset. Does that have anything to do with changing the RESET STATUS ( (I apologize for mentioning it as Boot Status earlier).)?

My specific question is: Why does the RESET STATUS not change when the watchdog is triggered?

vinisha_0-1731501511529.png

Best Regards,
Vinisha.

 

 

0 件の賞賛
返信

1,563件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

Did you modify that watchdog demo? I have tested that demo and the reset status is WDOG1.

Zhiming_Liu_0-1731546327097.png


Best Regards,
Zhiming

0 件の賞賛
返信

1,542件の閲覧回数
vinisha
Contributor I

Hello,

I have mentioned the watchdog demo code that we are using hear, kindly let me know is this any diffrent from your's

/*
 * Linux watchdog demo for LPC313x
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
 *
 */
#include <stdio.h>
#include <stdlib.h>
#include <sys/types.h>
#include <sys/stat.h>
#include <fcntl.h>
#include <getopt.h>
#include <string.h>
#include <errno.h>
 
#include <linux/watchdog.h>
 
#define WATCHDOGDEV "/dev/watchdog"
static const char *const short_options = "hd:i:";
static const struct option long_options[] = {
   {"help", 0, NULL, 'h'},
   {"dev", 1, NULL, 'd'},
   {"interval", 1, NULL, 'i'},
   {NULL, 0, NULL, 0},
};
 
static void print_usage(FILE * stream, char *app_name, int exit_code)
{
   fprintf(stream, "Usage: %s [options]\n", app_name);
   fprintf(stream,
      " -h  --help                Display this usage information.\n"
      " -d  --dev <device_file>   Use <device_file> as watchdog device file.\n"
      "                           The default device file is '/dev/watchdog'\n"
      " -i  --interval <interval> Change the watchdog interval time\n");
 
   exit(exit_code);
}
 
int main(int argc, char **argv)
{
   int fd;         /* File handler for watchdog */
   int interval;      /* Watchdog timeout interval (in secs) */
   int bootstatus;      /* Wathdog last boot status */
   char *dev;      /* Watchdog default device file */
 
   int next_option;   /* getopt iteration var */
   char kick_watchdog;   /* kick_watchdog options */
 
   /* Init variables */
   dev = WATCHDOGDEV;
   interval = 0;
   kick_watchdog = 0;
 
   /* Parse options if any */
   do {
      next_option = getopt_long(argc, argv, short_options,
                 long_options, NULL);

      fprintf(stdout, "next_option = %d\n", next_option);
      switch (next_option) {
      case 'h':
         print_usage(stdout, argv[0], EXIT_SUCCESS);
         fprintf(stdout, "interval = %d\n", interval);
      case 'd':
         dev = optarg;
         fprintf(stdout, "dev = %c\n", dev);
         break;
      case 'i':
         interval = atoi(optarg);
         fprintf(stdout, "interval = %d\n", interval);
         break;
      case '?':   /* Invalid options */
         print_usage(stderr, argv[0], EXIT_FAILURE);
         fprintf(stdout, "invalid option\n");
      case -1:   /* Done with options */
         fprintf(stdout, "DOne with option\n");
         break;
      default:   /* Unexpected stuffs */
         fprintf(stdout, "unexpected stuffs abort\n");
         abort();
      }
   } while (next_option != -1);
 
   /* Once the watchdog device file is open, the watchdog will be activated by
      the driver */
   fd = open(dev, O_RDWR);
   if (-1 == fd) {
      fprintf(stderr, "Error: %s\n", strerror(errno));
      exit(EXIT_FAILURE);
   }
 
   /* If user wants to change the watchdog interval */
   if (interval != 0) {
      fprintf(stdout, "Set watchdog interval to %d\n", interval);
      if (ioctl(fd, WDIOC_SETTIMEOUT, &interval) != 0) {
         fprintf(stderr,
            "Error: Set watchdog interval failed\n");
         exit(EXIT_FAILURE);
      }
   }
 
   /* Display current watchdog interval */
   if (ioctl(fd, WDIOC_GETTIMEOUT, &interval) == 0) {
      fprintf(stdout, "Current watchdog interval is %d\n", interval);
   } else {
      fprintf(stderr, "Error: Cannot read watchdog interval\n");
      exit(EXIT_FAILURE);
   }
 
   /* Check if last boot is caused by watchdog */
   if (ioctl(fd, WDIOC_GETBOOTSTATUS, &bootstatus) == 0) {
      fprintf(stdout, "Last boot is caused by : %s\n",
         (bootstatus != 0) ? "Watchdog" : "Power-On-Reset");
   } else {
      fprintf(stderr, "Error: Cannot read watchdog status\n");
      exit(EXIT_FAILURE);
   }
 
   /* There are two ways to kick the watchdog:
      - by writing any dummy value into watchdog device file, or
      - by using IOCTL WDIOC_KEEPALIVE
    */
   fprintf(stdout,
      "Use:\n"
      " <w> to kick through writing over device file\n"
      " <i> to kick through IOCTL\n" " <x> to exit the program\n");
   do {
      kick_watchdog = getchar();
      getchar(); // Consume the newline character after each input
      switch (kick_watchdog) {
      case 'w':
	 if (write(fd, "w", 1) == -1) {
            fprintf(stderr, "Error: Failed to write to watchdog device\n");
         } 
	 else {
            fprintf(stdout, "Kick watchdog through writing over device file\n");
	 }
     	 break;
      case 'i':
         ioctl(fd, WDIOC_KEEPALIVE, NULL);
         fprintf(stdout, "Kick watchdog through IOCTL\n");
         break;
      case 'x':
         fprintf(stdout, "Goodbye !\n");
         break;
      default:
         fprintf(stdout, "Unknown command\n");
         break;
      }
   } while (kick_watchdog != 'x');

   /* The 'V' value needs to be written into watchdog device file to indicate
      that we intend to close/stop the watchdog. Otherwise, debug message
      'Watchdog timer closed unexpectedly' will be printed
    */
   fprintf(stdout, "write v\n");
   write(fd, "V", 1);
   /* Closing the watchdog device will deactivate the watchdog. */
   close(fd);
}

 

Best Regards,

Vinisha

0 件の賞賛
返信

1,529件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

The watchdog test demo is this :

https://github.com/nxp-imx/imx-test/blob/lf-6.6.3_1.0.0/test/wdog/wdt_driver_test.c

The previous test case is M33 SDK watchdog demo using WDOG1. Are you using i.MX93 EVK from NXP?

Best Regards,
Zhiming

0 件の賞賛
返信

355件の閲覧回数
albe_merciai
Contributor I

I'm facing same issue using i.MX93 evk 11x11 from NXP, did you find any solution?

0 件の賞賛
返信