Hi Guys:
I noticed on imx8mm-evk board, qca9377 wifibt module is supported for android 10 (imx-android-10.0.0_1.0.0.tar.gz) while not supported in android 11(imx-android-11.0.0_2.4.0.tar.gz) or androd 12(imx-android-12.0.0_1.0.0.tar.gz).
I have a board basing on imx8mm soc and qca9377 wifibt module and would like to bring up the qca9377 wifibt module function under android 11 and android 12.
I have tried to port qca9377 wifi driver(qcacld-2.0) for android 10 (imx-android-10.0.0_1.0.0.tar.gz) to android 11 (imx-android-11.0.0_2.4.0.tar.gz), but there is a lot of buid errors caused by kernel upgraded. the changes I see so far are related to kernel core such as power management functions, time functions and DMA functions. I abandoned the effort as I see some change are critical and can not find the corresponding usages in new kernel API.
Can NXP render the support to qca9377 wifibt module in android 11/12 and higher android verson in future? Or where I can get the support from?
Best regards.
Johnson