IMX8X POR_N management

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8X POR_N management

ソリューションへジャンプ
1,108件の閲覧回数
vincent_massonn
Contributor IV
 
 
Hello,

I wanted to know if it was possible to make an assertion of the Power on reset of the IMX8X apart from the PMIC PF8100 / PF8200 (via a parallel secondary circuit).
Moreover in case of Power on reset on the IMX8X, the output SCU_WDOG_OUTSCU_WDOG_OUT is not asserted?

Thank you.
Best Regards Vincent Massonneau.
0 件の賞賛
返信
1 解決策
1,097件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi vincent_massonn

 

>I wanted to know if it was possible to make an assertion of the Power on reset of the
>IMX8X apart from the PMIC PF8100 / PF8200 (via a parallel secondary circuit).

in general yes, one can use some gpio for controlling such external circut.

>Moreover in case of Power on reset on the IMX8X, the output
>SCU_WDOG_OUTSCU_WDOG_OUT is not asserted?

it depends on reset type, for case "partition" reset it is not asserted as described on below


https://community.nxp.com/t5/i-MX-Processors/Watchdog-AP-cores-on-imx8QM-MEK/m-p/1153684

 

Types of reset are described in sect.13.7 TIMER: Timer Service sc_fw_api_qx_b0.pdf

included in SCFW Porting Kit​

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,098件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi vincent_massonn

 

>I wanted to know if it was possible to make an assertion of the Power on reset of the
>IMX8X apart from the PMIC PF8100 / PF8200 (via a parallel secondary circuit).

in general yes, one can use some gpio for controlling such external circut.

>Moreover in case of Power on reset on the IMX8X, the output
>SCU_WDOG_OUTSCU_WDOG_OUT is not asserted?

it depends on reset type, for case "partition" reset it is not asserted as described on below


https://community.nxp.com/t5/i-MX-Processors/Watchdog-AP-cores-on-imx8QM-MEK/m-p/1153684

 

Types of reset are described in sect.13.7 TIMER: Timer Service sc_fw_api_qx_b0.pdf

included in SCFW Porting Kit​

 

Best regards
igor

0 件の賞賛
返信