IMX8X ADC_IN0 Configuration Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8X ADC_IN0 Configuration Problem

1,020件の閲覧回数
jack_huang1
Contributor III

Dear:

       In IMX8QX scheme, ADC_IN0 needs to be multiplexed as GPIO. When configured as output, no matter the output is 0 or 1, the voltage on the pin does not change. The configuration is as follows: 

        SC_P_ADC_IN0_LSIO_GPIO1_IO10 0x0600006C /*phy1_reset*/

         or

          SC_P_ADC_IN0_LSIO_GPIO1_IO10 0x0600004C /*phy1_reset*/

       Please confirm whether there is a problem when ADC_IN0 is reused as gpio. Because other pins we normally configure for gpio multiplexing have no problem, but now this ADC_IN0 after multiplexing control has no reaction?

        Thank you!

         Best Regards!

          

0 件の賞賛
返信
2 返答(返信)

1,000件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

968件の閲覧回数
jack_huang1
Contributor III

Dears:

          The problem has been solved. Thanks!

 

Best  Regards!

0 件の賞賛
返信