IMX8ULP Boundary Scan EXTEST issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8ULP Boundary Scan EXTEST issues

1,457 Views
Corebb
Contributor I

I have an IMX8ULP chip, and I want to use JTAG for Boundary Scan.

I can successfully connect and run in SAMPLE mode, and I can see the IO status. However, when I switch to EXTEST mode, the connection immediately drops, and it seems like the chip powers off and resets right away.

I saw documentation related to the IMX8M PLUS that mentions the need to set PMIC_STBY_REQ to low, and several BOOT_MODE pins need to be configured to different states.

lQLPKd43qVdrMqvNAt3NAuGw509gEsoKdXUG7Zcu1KpmAQ_737_733.png

But in the IMX8ULP, this part is omitted, and I couldn't find any reference in the documentation about whether the BOOT_MODE needs to be set to a specific state. I also don't know how to set PMIC_STBY_REQ to low.

QQ20241017-162302.png

My request is to enter EXTEST mode in Boundary Scan on the IMX8ULP(MIMX8UD7CVP08SC) and control the IO levels. I need help to check if any specific pins need to be configured in a certain state to achieve this. If so, how should this be done? Thank you.

0 Kudos
Reply
3 Replies

1,371 Views
Corebb
Contributor I

Need Help.

0 Kudos
Reply

1,430 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

JTAG is different from MX8MPlus then

JTAG_TDO -> JTAG_TDI

JTAG_TDI -> JTAG_TCK

JTAG_TCK -> JTAG_TDO

 

JTAG should work with these changes.

Regards

0 Kudos
Reply

1,423 Views
Corebb
Contributor I
Do you mean i need to change the JTAG connection from TDO to TDI, TDI to TCK, TCK to TDO?

Why is that?
Originally, i can connect, and get the IDCode succeesfully without change the connection.

After change it just like you said, it even can't connect.


The only problem I originally have, is it can't enter the EXTEST mode, it just like the chip reset when i send EXTEST command.
0 Kudos
Reply