IMX8QuadXPlus LPDDR4 CA SWAP in Channel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QuadXPlus LPDDR4 CA SWAP in Channel

ソリューションへジャンプ
4,437件の閲覧回数
Wenhai_05
Contributor I

Dear

Could you confirm if there is any restriction of CA(Command & Address) swapping on LPDDR4?

Thanks!

BR

Alex

 

0 件の賞賛
返信
1 解決策
4,428件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Swapping of the CA lines is not supported.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,433件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

As long as it complies with JEDEC specifications,no special. The details design you can refer to our hardware user guide document.

0 件の賞賛
返信
4,430件の閲覧回数
Wenhai_05
Contributor I

Dear

It is not stated in JEDEC specification. I think it depends on the features of DDR PHY and Controller.

As I know, IMX8QXP support data bus swapping. I can fill in my data configuration to get corresponding code. Refer to attachment, which is snapped in worksheet (BoardDataBusConfig) of  MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_V15.xlsx.

Similarly, due to layout, I have the requirement of CA swapping. Such as, DDR_DCF00 is configured to CA2_A, I want to configure it as CA5_A.

There are not these information in user guide .

Thanks!

BR

Alex

0 件の賞賛
返信
4,429件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Swapping of the CA lines is not supported.

0 件の賞賛
返信