【IMX8QXP,SJA1105Q】device tree config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

【IMX8QXP,SJA1105Q】device tree config

Jump to solution
2,005 Views
jianwei_lan
Contributor III

Dear friend

My platform is i.MX8QXP, SJA1105, Yocto L5.4.70_2.3.0.

description:

1)SJA1105's port0 connect to i.MX8QXP's ethphy0,

2)SJA1105's SPI connect to i.MX8QXP's LSPI2;

Question:

1)can you provide an device tree example for SJA1105 connected to i.MX8QXP according to my description? 

 

----

BR

0 Kudos
Reply
1 Solution
1,995 Views
joanxie
NXP TechSupport
NXP TechSupport

all of SJA1105Q materials you can find from the link as below, you can refer to the dts file as below:

"https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree"

View solution in original post

0 Kudos
Reply
1 Reply
1,996 Views
joanxie
NXP TechSupport
NXP TechSupport

all of SJA1105Q materials you can find from the link as below, you can refer to the dts file as below:

"https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree"

0 Kudos
Reply