【IMX8QXP,SJA1105Q】device tree config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

【IMX8QXP,SJA1105Q】device tree config

ソリューションへジャンプ
2,008件の閲覧回数
jianwei_lan
Contributor III

Dear friend

My platform is i.MX8QXP, SJA1105, Yocto L5.4.70_2.3.0.

description:

1)SJA1105's port0 connect to i.MX8QXP's ethphy0,

2)SJA1105's SPI connect to i.MX8QXP's LSPI2;

Question:

1)can you provide an device tree example for SJA1105 connected to i.MX8QXP according to my description? 

 

----

BR

0 件の賞賛
返信
1 解決策
1,998件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

all of SJA1105Q materials you can find from the link as below, you can refer to the dts file as below:

"https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree"

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,999件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

all of SJA1105Q materials you can find from the link as below, you can refer to the dts file as below:

"https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree"

0 件の賞賛
返信