IMX8QXP RMII KSZ8041

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QXP RMII KSZ8041

1,513件の閲覧回数
Chethanbg
Contributor III

Hi,

Currently in RMII mode we are using 25 Mhz crystal mode

The KSZ8041RNL generates the 50MHz RMII REF_CLK and outputs it to the MAC

attached is the block diagram for your reference.

In pin configuration RGMII_TXC should be configured as ENET0_RCLK50M_IN input  right?

IMX8QXP_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_IN                               0x06000061

 

Also let us know the pad settings  0x06000061 is correct

0 件の賞賛
返信
1 返信

1,495件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Chethanbg,

I hope you are doing well.

Your understanding is correct and the pad settings also seem to be correct.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信