IMX8QXP MIPI CSI voltage level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QXP MIPI CSI voltage level

5,006件の閲覧回数
YK7
Contributor I

Hi

I would like to connect the MIPI-CSI 4-lanes interfaces of iMX8 QXP to a CSI-2 bridge (i.e. lattice LIF-MD6000) to receive parallel raw pixels data from sensor. However, I am quite confuse as the IO supplies for its MIPI PHY and GPIO are 1V on VDD_MIPI_1P0 pins and 1.8V on VDD_MIPI_1P8 pins. Based on MIPI CSI-2 standards, 1.2V is the typical/common D-PHY voltage supply to work with.

Would the intended electrical connections be an issue? What can be the workaround solution?

Thanks.

Rdgs,
YK

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

5,002件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi YK

 

if bridge complies with MIPI CSI2 Specification V1.3, MIPI D-PHY specification V1.2

it can be connected with i.MX8M Mini.

Regarding : " IO supplies for its MIPI PHY and GPIO are 1V on VDD_MIPI_1P0 pins and 1.8V on VDD_MIPI_1P8 pins" - this rule is applicable to GPIO signals, their levels are defined by pad

power supply value.

 

Best regards
igor

0 件の賞賛
返信

4,994件の閲覧回数
YK7
Contributor I

Hi Igor,

I am using I.MX8 QXP.

What MIPI specs or standards can its MIPI CSI interfaces be connected with?

You had mentioned the IO supplies of the 2 MIPI power rails are meant for GPIO signals. Can I say that when mux pin use as MIPI CSI2, those differential MIPI data and clock signals would match the external D-PHY operating at 1.2V?

 

Rdgs, YK

0 件の賞賛
返信

4,983件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>What MIPI specs or standards can its MIPI CSI interfaces be connected with?

 

MIPI CSI2 Specification V1.3, MIPI D-PHY specification V1.2)

 

>You had mentioned the IO supplies of the 2 MIPI power rails are meant for GPIO signals.

 

sorry I did not answer that.

 

>Can I say that when mux pin use as MIPI CSI2, those differential MIPI data and clock signals would match >the external D-PHY operating at 1.2V?

 

they match values defined in MIPI CSI2 Specification V1.3, MIPI D-PHY specification V1.2)

 

Best regards
igor

0 件の賞賛
返信